earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 警报
产品版本: 2.0, 2.1, 3.0, 3.1
2018/5/18

SNMP Notification Distribution Method

SNMP alarms are typically used when the alarm receiver does not have access to the EcoStruxure Building Operation software or when a central unit, for example the IT department, wants to collect alarms from different sources in one place.

You can send notifications as SNMP traps from any EcoStruxure BMS server using SNMP version 3. The EcoStruxure BMS server can send one or many traps depending on the setting.

You configure the SNMP trap to send the notification message.

Notifications sent using SNMP trap are written to the event log.

SNMP is also used to send information regarding the status of a SmartX server. 有关更多信息,请参阅 SmartX Servers ..

  • Notification Distribution Methods
  • Create Notification Wizard - Configure SNMP Page
  • SmartX Servers
  • Email Notification Distribution Method
  • Write to File Notification Distribution Method