earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Server, Virtual Project Servers
Functionalities: Alarms
Product version: 1.8
10/13/2016

Create Alarm Triggered Notification Wizard – Configure Alarm Triggered Notification Page

Use the Configure Alarm Triggered Notification page to create an alarm triggered notification.

 
action_zoom_plus_stroke Configure Alarm Triggered Notification page
Figure: Configure Alarm Triggered Notification page

Table: Alarm Triggered Notification Page

Property

Description

Status

Select Disabled to deactivate the notification function.

Activation schedule

Enter the schedule that contains the value that activates the notification.

Schedule value when active

Enter the value, generated by the connected schedule or other multistate variable, that activates the notification.

Report template

Enter the path to the report template.

For more information, see Notification Reports .

Decimal symbo l

Select the decimal symbol to be used in the notification and the notification report template.

Localization

Select a language among the language packs installed on the SmartStruxure server.

Notification text

Edit the notification text.

Quick filter

Enter a word to filter on. For more information, see Quick Filter ..

Substitution codes list

Add the substitution codes you want to use in the notification or notification report.

For more information, see Alarm Substitution Codes .

Substitute missing data with

Enter the text that is displayed when a value is missing. By default, a missing value displays nothing at all.

 
action_zoom_plus_stroke

Add

Click to add a distribution method to the notification.

For more information, see Notification Distribution Methods .

 
action_zoom_plus_stroke

Edit

Click to configure the selected distribution method in the notification.

For more information, see Notification Distribution Methods .

 
action_zoom_plus_stroke

Remove

Click to remove the selected distribution method from the notification.

For more information, see Notification Distribution Methods .

 
action_zoom_plus_stroke

Add condition

Click to add a condition that has to be met for the notification to be displayed or sent.

For more information, see Alarm Filter Conditions .

 
action_zoom_plus_stroke

Remove condition

Click to remove a condition that has to be met for the notification to be displayed or sent.

For more information, see Alarm Filter Conditions .

 
action_zoom_plus_stroke

Add row

Click to add a row to the condition.

 
action_zoom_plus_stroke

Remove row

Click to remove the row from the condition.

 
action_zoom_plus_stroke

Clear all

Click to clear the selected conditions.

  • Notifications
  • Alarm Triggered Notification View
  • Notification Reports
  • Quick Filter
  • Alarm Substitution Codes
  • Notification Distribution Methods
  • Alarm Filter Conditions
  • Create Variable Triggered Notification Wizard – Configure Variable Triggered Notification Page