earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Server, Virtual Project Servers
Functionalities: Alarms
Product version: 1.8
10/13/2016

Variable Triggered Notification View

Use the Variable Triggered Notification view to view and edit the configuration of a variable triggered notification.

 
action_zoom_plus_stroke Variable triggered notification view
Figure: Variable triggered notification view

Table: Variable Triggered Notification View

Number

Description

 
action_zoom_plus_stroke

Properties

Use the properties to configure how the notification should be activated, for the report template connected to the notification, and for notification text properties. For more information, see Variable Triggered Notification Properties - Basic Tab ..

 
action_zoom_plus_stroke

Notification text

Use the notification text to edit the contents and formatting of the notification text. For more information, see Notifications ..

 
action_zoom_plus_stroke

Quick filter

Use the quick filter to enter a word to filter the alarm substitution codes on. For more information, see Quick Filter ..

 
action_zoom_plus_stroke

Substitution codes list

Use the Report @(Report) substitution code to write the notification report text in the notification.

 
action_zoom_plus_stroke

Distribution method

Use the distribution method to start a wizard where you select how the notification is distributed. For more information, see Notification Distribution Methods ..

  • Notifications
  • Create Variable Triggered Notification Wizard – Configure Variable Triggered Notification Page
  • Variable Triggered Notification Properties - Basic Tab
  • Notification Reports
  • Quick Filter
  • Create Notification Wizard - Configure Email Page
  • Create Notification Wizard - Configure SNMP Page
  • Create Notification Wizard - Configure Write to File Page