earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Alarmas
Versión del producto: 2023, 2024, 7.0
16/12/2022

Create Notification Wizard - Configure SNMP Page

Use the Configure SNMP page to configure the SNMP properties of the notification.

 
action_zoom_plus_stroke Configure SNMP page
Figura: Configure SNMP page

Tabla: Configure SNMP Page

Component

Description

Address

Type the address to the SNMP manager that receives the notification.

Port

Type the port that is used by the SNMP manager that receives the notification.

User name

Type the user name of the user on the SNMP manager that receives the notification.

Security level

Select the security level.

Authentication protocol

Select the authentication level:

  • SHA-1

  • MD5

Authentication password

Enter the password of the user on the SNMP manager that is to receive the notification.

Confirm password

Type the password again.

Privacy encryption protocol

Enter the privacy encryption protocol of the user on the SNMP manager that is to receive the notification:

  • AES-128

  • DES

Privacy password

Enter the privacy password used to encrypt the message being sent.

Confirm password

Type the password again.

  • Notification Distribution Methods
  • Creating an Alarm Triggered Notification
  • Configuring an Alarm Triggered Notification 
  • Creating a Variable Triggered Notification
  • Configuring a Variable Triggered Notification
  • Alarm Triggered Notification View
  • Variable Triggered Notification View