Use the Configure Write to File page to configure the write to file properties of the notification.
Component |
Description |
File name |
Type a name for the file. |
![]() |
Click to open the Configure dialog box where you configure a reference for a dynamic file name. For more information, see Configure Dialog Box – Configuration Tab . |
Uniquenes s |
Select whether to append or prepend a timestamp to the file name, or generate the file without any timestamp. The timestamp in the file name is expressed in UTC. |
Overwrite |
Select True to overwrite the file when a new file is generated. |