earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server, AS-B, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Alarms
Product version: 1.9
10/12/2017

Properties and Watch Substitution Codes

Properties and Watch substitution codes represent the information you want to display when a notification report is triggered. The information is dynamically filled in from the properties or Watch data that are included in the notification report.

Table: Properties Substitution Codes for Notification Reports

Code

Description

@(DisplayName)

Writes the property display name.

@(ObjectName)

Writes the name of the object that has the property.

@(ObjectPath)

Writes the path of the object that has the property.

@(PropertyName)

Writes the property name.

@(Unit)

Writes the property unit.

@(Value)

Writes the property value.

  • Notification Reports
  • Events Substitution Codes
  • Trend Logs Substitution Codes