功能: 警报
产品版本: 1.8
2016/10/13

Properties Substitution Codes

Properties substitution codes represent the information you want to display when a notification report is triggered. The information is dynamically filled in from the properties that are included in the notification report.

表格: Properties Substitution Codes for Notification Reports

Code

Description

@(DisplayName)

Writes the property display name.

@(ObjectName)

Writes the name of the object that has the property.

@(ObjectPath)

Writes the path of the object that has the property.

@(PropertyName)

Writes the property name.

@(Unit)

Writes the property unit.

@(Value)

Writes the property value.

  • Notification Reports
  • Trend Logs Substitution Codes