earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 警报
产品版本: 2.0, 2.1, 3.0, 3.1
2020/3/17

Properties and Watch View Properties Substitution Codes

Properties and watch view properties substitution codes represent the information you want to display when a notification report is triggered. The information is dynamically filled in from the properties or watch view properties data that are included in the notification report.

表格: Properties and Watch View Properties Substitution Codes for Notification Reports

Code

Description

@(DisplayName)

Writes the property display name.

@(ObjectName)

Writes the name of the object that has the property.

@(ObjectPath)

Writes the path of the object that has the property.

@(PropertyName)

Writes the property name.

@(Unit)

Writes the property unit.

@(Value)

Writes the property value.

  • Notification Reports
  • Alarm Substitution Codes
  • Events Substitution Codes
  • Trend Log Records Substitution Codes