earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Explicación de procesos

Explicación de procesos


Productos Enterprise Server
Funcionalidades: Ingeniería
Versión del producto: 1.8, 1.9
07/12/2015

Resolving Enterprise Server Port Conflicts

You resolve Enterprise Server port conflicts so that users can log on to the Building Operation system

Mostrar más
action_close

​The Software Administrator installs with the Enterprise Server installation package. You use the Software Administrator to start and stop the server service and configure the ports of the Enterprise Server.

Other server settings, for example e-mail service, time, and time zone settings are configured through WorkStation.

Service

The Enterprise Server runs in the background as a Windows service. You start and stop the server service through the Software Administrator or Windows Service. Before shutting down the server, make sure the stop does not negatively affect your site.

Ports

The Enterprise Server uses HTTP and TCP protocols to communicate with other servers and clients. In the Software Administrator, you configure the port number of each protocol the server listens to when communicating through a specific protocol.

To configure a protocol port number, you first have to stop the running Enterprise Server service.

Aviso

Port changes you have made using Software Administrator are not automatically updated in the Communication view for SmartStruxure servers.

Database Location

In the Software Administrator, you find the path to the location where the Enterprise Server writes and stores data and objects that are created by either the Enterprise Server or the user.

Enterprise Server System Log

The Enterprise Server System log contains events logged by the Enterprise Server. Examples of logged events are start up sequence, port settings, failures, run time, and current server status.

To resolve Enterprise Server port conflicts
  1. Start Software Administrator.

  2. On the Enterprise Server tab, click the Stop Service button.

  3. Check the HTTP Port , HTTPS Port , and TCP Port boxes to ensure that there are no port conflicts indicated by a red border around the port number box.

     
    action_zoom_plus_stroke
  4. If necessary, change the conflicting port number.

  5. Click the Start Service button.

  6. Click OK .

  • Installation Overview
  • Software Administrator
  • Log On Methods
  • Software Administrator – Enterprise Server View
  • Failed to access the server, a network error occurred