earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Server, Project Configuration Tool
功能: 警报
产品版本: 1.8
2016/10/13

Alarm Triggered Notification View

Use the Alarm Triggered Notification view to view and edit the configuration of an alarm triggered notification.

 
action_zoom_plus_stroke Alarm triggered notification view
图: Alarm triggered notification view

表格: Alarm Triggered Notification View

Number

Description

 
action_zoom_plus_stroke

Properties

Use the properties to configure how the notification is activated, what notification report to connect to the notification, and what properties to use for the notification text. 有关更多信息,请参阅 Alarm Triggered Notification Properties - Basic Tab ..

 
action_zoom_plus_stroke

Notification text

Use the notification text to edit the contents and formatting of the notification text. 有关更多信息,请参阅 Notifications ..

 
action_zoom_plus_stroke

Quick filter

Use the Quick filter to enter a word to filter on. 有关更多信息,请参阅 Quick Filter ..

 
action_zoom_plus_stroke

Substitution codes list

Use the alarm substitution codes list to select the data you want to include in the notification. 有关更多信息,请参阅 Alarm Substitution Codes ..

 
action_zoom_plus_stroke

Distribution method

Use the distribution method to start a wizard where you configure how the notification is distributed.

有关更多信息,请参阅 Create Notification Wizard - Configure Email Page .

有关更多信息,请参阅 Create Notification Wizard - Configure SNMP Page .

有关更多信息,请参阅 Create Notification Wizard - Configure Write to File Page .

 
action_zoom_plus_stroke

Filter Settings

Use the filter settings to select the alarm filter conditions that have to be met before the notification is triggered. 有关更多信息,请参阅 Alarm Filter Conditions ..

  • Notifications
  • Create Alarm Triggered Notification Wizard – Configure Alarm Triggered Notification Page
  • Alarm Triggered Notification Properties - Basic Tab
  • Notification Reports
  • Quick Filter
  • Alarm Substitution Codes
  • Create Notification Wizard - Configure Email Page
  • Create Notification Wizard - Configure SNMP Page
  • Create Notification Wizard - Configure Write to File Page
  • Alarm Filter Conditions