earth_america
user_standard Anmelden
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Benutzeroberfläche

Benutzeroberfläche


Produkte: AS-C, AS-B, Enterprise Server, AS-P, Projekt Configuration Server, Project Configuration Tool
Funktionen: Alarme
Produktversion: 1.8
13.10.2016

Create Variable Triggered Notification Wizard – Configure Variable Triggered Notification Page

Use the Configure Variable Triggered Notification page to create a variable triggered notification.

 
action_zoom_plus_stroke Configure Variable Triggered Notification page
Abbildung: Configure Variable Triggered Notification page

Tabelle: Configure Variable Triggered Notification Page

Property

Description

Trigger variable

Enter the variable that triggers the notification.

Trigger condition

Select when you want the notification to be triggered: when the trigger variable changes to true, changes to false, or all changes.

Report template

Enter the path to the report template.

Für weitere Informationen siehe Notification Reports .

Generate report relative to

Enter the path to the object that is relative to the generated notification report.

Decimal symbol

Select the decimal symbol to be used in the notification and the notification report template.

Localization

Select a language among the language packs installed on the SmartStruxure server.

Notification text

Edit the notification text.

Quick filter

Enter a word to filter on. Für weitere Informationen siehe Quick Filter ..

Substitution codes list

Use the Report @(Report) substitution code to write the notification report text in the notification.

 
action_zoom_plus_stroke

Add

Click to add a distribution method to the notification.

Für weitere Informationen siehe Notification Distribution Methods .

 
action_zoom_plus_stroke

Edit

Click to configure the selected distribution method in the notification.

Für weitere Informationen siehe Notification Distribution Methods .

 
action_zoom_plus_stroke

Remove

Click to remove the selected distribution method from the notification.

Für weitere Informationen siehe Notification Distribution Methods .

  • Notifications
  • Variable Triggered Notification View
  • Notification Reports
  • Quick Filter
  • Notification Distribution Methods
  • Create Alarm Triggered Notification Wizard – Configure Alarm Triggered Notification Page