earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interface utilisateur

Interface utilisateur


Produits : AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Fonctionnalités : Alarmes
Version produit : 2.0, 2.1, 3.0, 3.1
15/01/2019

Create Variable Triggered Notification Wizard – Configure Variable Triggered Notification Page

Use the Configure Variable Triggered Notification page to create a variable triggered notification.

 
action_zoom_plus_stroke Configure Variable Triggered Notification page
Figure : Configure Variable Triggered Notification page

Table : Configure Variable Triggered Notification Page

Property

Description

Trigger variable

Enter the variable that triggers the notification.

Trigger condition

Select when you want the notification to be triggered: when the trigger variable changes to true, changes to false, or all changes.

Report template

Enter the path to the report template.

Pour plus d'informations, voir Notification Reports .

Generate report relative to

Enter the path to the object that is relative to the generated notification report.

Decimal symbol

Select the decimal symbol to be used in the notification and the notification report template.

Localization

Select a language among the language packs installed on the EcoStruxure BMS server.

Notification text

Edit the notification text.

Quick filter

Enter a word to filter on. Pour plus d'informations, voir Filtre rapide ..

Substitution codes list

Use the Report @(Report) substitution code to write the notification report text in the notification.

 
action_zoom_plus_stroke

Add

Click to add a distribution method to the notification.

Pour plus d'informations, voir Notification Distribution Methods .

 
action_zoom_plus_stroke

Edit

Click to configure the selected distribution method in the notification.

Pour plus d'informations, voir Notification Distribution Methods .

 
action_zoom_plus_stroke

Remove

Click to remove the selected distribution method from the notification.

Pour plus d'informations, voir Notification Distribution Methods .

  • Notifications
  • Variable Triggered Notification View
  • Notification Reports
  • Filtre rapide
  • Notification Distribution Methods
  • Create Alarm Triggered Notification Wizard – Configure Alarm Triggered Notification Page