earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos AS-B
Funcionalidades: Hardware
Versión del producto: 1.8, 1.9
16/02/2018

AS-B Communication Ports

AS-B has the following communication ports:

  • 2 Ethernet 10/100 megabit ports

  • 1 RS-485 port

  • 1 USB host port

  • 1 USB device port

The following table describes the ports that are available with AS-B.

Tabla: AS-B Communication Ports

Communication port

Connection

Ethernet 1 10/100

IP, LAN/WAN, Modbus, BACnet

Ethernet 2 10/100

IP, LAN/WAN, Modbus, BACnet

RS-485

Modbus, BACnet

USB host

USB device

Device Administrator

There is one USB host port to connect to external devices, such as ADs, telephone modems, printers, memory expansions (USB sticks or hard disc drives), and expansion modules. The USB device port on the front is intended for program download from a PC by means of Device Administrator. The port is connected to a PC or a downstream port of a hub.

The Ethernet communication is performed over a 10/100BaseTX, 10 or 100 Mbit/s, twisted pair network. AS-B has a built-in Ethernet switch with two ports connected to two RJ45 connectors. One port should be connected to the site network. The other port can be used to connect a single WorkStation or WebStation, a Modbus TCP unit, or a BACnet/IP device, but not another SmartStruxure server. By default, both ports are enabled for use. The Ethernet 2 port can be disabled if needed.

  • Hardware Overview
  • AS-Bs
  • AD v1
  • AD v2