earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos AS-B
Funcionalidades: Hardware
Versión del producto: 3.2
10/06/2022

SmartX AS-B Server Communication Ports

A SmartX AS-B server has the following communication ports:

  • 2 Ethernet 10/100 megabit ports

  • 1 RS-485 port

  • 1 USB host port

  • 1 USB device port

Tabla: SmartX AS-B Server Communication Ports

Communication port

Connection

Ethernet 1 10/100

IP, LAN/WAN, Modbus, BACnet

Ethernet 2 10/100

IP, LAN/WAN, Modbus, BACnet

RS-485

Modbus, BACnet

USB host

SmartX Advanced Display (AD), Wireless Adapter - Advanced

USB device

Device Administrator

The Ethernet communication is performed over a 10/100BaseTX, 10 or 100 Mbit/s, twisted pair network. The SmartX AS-B servers have two Ethernet ports with RJ45 connectors.

The two Ethernet ports can be configured in three different modes: switching enabled, second port disabled, or dual IP networks. One port should be connected to the site network. When switching between the two ports is enabled, the other port can be used to connect computers running WorkStation or WebStation, Modbus TCP units, or BACnet/IP devices such as MP Series controllers, but not another EcoStruxure BMS server. To limit access to the system, you can disconnect the second port. When the two ports are configured in dual IP mode, you can connect a separate network of MP Series controllers to the second port and the SmartX server can be configured as a DHCP server. You can lock the private DHCP network on the second port to select which DHCP clients can communicate with the DHCP server.

The USB host port can be used for connecting devices such as the SmartX Advanced Display (AD) and Wireless Adapter - Advanced. Para obtener más información, consulte Connecting AD v3 to a SmartX Server and a 24 VDC Power Supply .Para obtener más información, consulte Wireless Adapter - Advanced .

The USB device port is intended for program download from a PC by means of Device Administrator. The port is connected to a PC or a downstream port of a hub.

  • Hardware Overview
  • SmartX AS-B Servers
  • Connecting AD v3 to a SmartX Server and a 24 VDC Power Supply
  • AD v3
  • Wireless Adapter - Advanced