SmartX AS-B servers use pluggable terminal blocks, which are easy to install and remove from the device. The terminal blocks are delivered with the device.
Spare terminal blocks can be ordered using the part number SXWASBCON10001.
The wiring recommendations are provided separately. For more information, see Wiring .
SmartX AS-B servers with 24 I/O points use nine pluggable terminal blocks and one fixed terminal block.
For more information, see Screw Terminals for SmartX AS-B Servers with 24 I/O Points .
SmartX AS-B servers with 36 I/O points use nine pluggable terminal blocks and one fixed terminal block.
For more information, see Screw Terminals for SmartX AS-B Servers with 36 I/O Points .