SmartX AS-B servers use pluggable terminal blocks, which are easy to install and remove from the device. The terminal blocks are delivered with the device.
Spare terminal blocks can be ordered using the part number SXWASBCON10001.
The wiring recommendations are provided separately. Para obtener más información, consulte Wiring .
SmartX AS-B servers with 24 I/O points use nine pluggable terminal blocks and one fixed terminal block.
Para obtener más información, consulte Screw Terminals for SmartX AS-B Servers with 24 I/O Points .
SmartX AS-B servers with 36 I/O points use nine pluggable terminal blocks and one fixed terminal block.
Para obtener más información, consulte Screw Terminals for SmartX AS-B Servers with 36 I/O Points .