AS-B servers use pluggable terminal blocks, which are easy to install and remove from the device. The terminal blocks are delivered with the device.
Spare terminal blocks can be ordered using the part number SXWASBCON10001.
The wiring recommendations are provided separately. Więcej informacji zawiera Wiring .
AS-B servers with 24 I/O points use nine pluggable terminal blocks and one fixed terminal block.
Więcej informacji zawiera Screw Terminals for AS-B Servers with 24 I/O Points .
AS-B servers with 36 I/O points use nine pluggable terminal blocks and one fixed terminal block.
Więcej informacji zawiera Screw Terminals for AS-B Servers with 36 I/O Points .