earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-B
功能: 硬件
产品版本: 1.8, 1.9
2020/2/6

AS-B Screw Terminals

AS-B uses pluggable terminal blocks, which are easy to install and remove from the device. The terminal blocks are delivered with the device.

Spare terminal blocks can be ordered using the part number SXWASBCON10001.

The following sections describe the screw terminals for the different AS-B models. The wiring recommendations are provided separately. 有关更多信息,请参阅 Wiring .

Screw Terminals for AS-Bs with 24 I/O Points

AS-Bs with 24 I/O points use nine pluggable terminal blocks and one fixed terminal block.

有关更多信息,请参阅 Screw Terminals for AS-Bs with 24 I/O Points .

Screw Terminals for AS-Bs with 36 I/O Points

AS-Bs with 36 I/O points use nine pluggable terminal blocks and one fixed terminal block.

有关更多信息,请参阅 Screw Terminals for AS-Bs with 36 I/O Points .

  • AS-Bs
  • Screw Terminals for AS-Bs with 24 I/O Points
  • Screw Terminals for AS-Bs with 36 I/O Points
  • Wiring