earth_america
user_standard Accedi
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaccia dell'utente

Interfaccia dell'utente


Prodotti: AS-B
Funzionalità: Hardware
Versione del prodotto: 1.8, 1.9
29/01/2018

AS-B LEDs

arrow1_rotationStatus LED arrow1_rotationRS-485 LEDs arrow1_rotationEthernet LEDs

There are five LEDs on the front panel of AS-B.

 
action_zoom_plus_stroke AS-B LEDs
Figura: AS-B LEDs

Tabella: The Five LEDs

Function

Color

Status (AS-B)

Green/Red

RS-485 Tx

Yellow

RS-485 Rx

Green

Ethernet 1

Green/Yellow

Ethernet 2

Green/Yellow

Avviso
  • The AS-B Ethernet and Status indicators comprise two LEDs (green/yellow and green/red respectively) in one structure. Normally, when one LED is lit, the other is not lit and vice versa, that is, the indicator will show one color at a time.

The LEDs indicate status of AS-B and the ongoing communication.

Status LED

The Status LED on the front of the SmartStruxure devices changes color and flashes to indicate the status of the device.

Per maggior informazioni, consulta Status LEDs .

RS-485 LEDs

The RS-485 LEDs indicate the condition of the RS-485 communication according to the following table.

Tabella: RS-485 LED Patterns

LED Patterns

Condition

Yellow, flashing (Tx)

Transmit data

Green, flashing (Rx)

Receive data

Ethernet LEDs

The Ethernet (1 and 2) LEDs indicate the condition of the Ethernet communication according to the following table.

Tabella: Ethernet LED Patterns

LED Patterns

Condition

Green, flashing

10 Mbit communication

Yellow, flashing

100 Mbit communication

  • AS-Bs
  • Status LEDs