earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interface de utilizador

Interface de utilizador


Produtos: AS-B
Funcionalidades: Hardware
Versão do produto: 3.3, 2022, 2023, 2024
23-04-2024

AS-B Server LEDs

arrow1_rotationStatus LED arrow1_rotationRS-485 LEDs arrow1_rotationEthernet LEDs

There are five LEDs on the front panel of the AS-B server.

 
action_zoom_plus_stroke  AS-B server LEDs
Imagem: AS-B server LEDs

Tabela: The Five LEDs

Function

Color

Status (AS-B)

Green/Red

RS-485 Tx

Yellow

RS-485 Rx

Green

Ethernet 1

Green/Yellow

Ethernet 2

Green/Yellow

Nota

The AS-B server Ethernet and Status indicators comprise two LEDs (green/yellow and green/red respectively) in one structure. Normally, when one LED is lit, the other is not lit and vice versa, that is, the indicator will show one color at a time.

The LEDs indicate status of the AS-B server and the ongoing communication.

Status LED

The automation server Status LED indicates the condition of the device.

Tabela: Automation Server Status LED Patterns

LED Patterns

Condition

Green, constant

Normal operation, status OK

Green, flashing (~1 Hz)

Device restarting, wait

Green, flashing (~10 Hz)

Device shutting down

Red, constant

Detected error, attention required

Red, flashing (~1 Hz)

Device operates, but a problem needs attention

Red/green, flashing (~1 Hz)

Device firmware upgrade (DFU) mode or firmware being downloaded in DFU mode

No light

No input power

RS-485 LEDs

The RS-485 LEDs indicate the condition of the RS-485 communication.

Tabela: RS-485 LED Patterns

LED Patterns

Condition

Yellow, flashing (Tx)

Transmit data

Green, flashing (Rx)

Receive data

Ethernet LEDs

The Ethernet (1 and 2) LEDs indicate the condition of the Ethernet communication.

Tabela: Ethernet LED Patterns

LED Patterns

Condition

Green, flashing

10 Mbit communication

Yellow, flashing

100 Mbit communication

  • AS-B Servers
  • Status LEDs