The output override function allows you to manually override outputs. This function can be used for testing, commissioning, and maintenance of equipment.
An override display unit consisting of an LCD display and five keys is provided for override control of the output channels.
The override display also enables you to perform the following actions:
View inputs and outputs
Configure inputs and outputs
The override display has a menu-driven user interface, which facilitates overriding of the outputs, local configuration of inputs and outputs, and other tasks.
Więcej informacji zawiera User Experience .
You use the keys on the override display to navigate the screens of the user interface and to select options on menus and lists.
Więcej informacji zawiera Keys .
The basic operation of the user interface includes the following actions:
Highlight an option on a menu or list
Select an option on a menu or list
Change a value
Więcej informacji zawiera Basic Operation .
You use the override display to manually override digital outputs as well as analog outputs.
Więcej informacji zawiera Override Outputs .
Using the override display, you can view the configuration and the present values for inputs and outputs, and for outputs you can also view the override status.
Więcej informacji zawiera View Inputs and Outputs .
In configuration mode, you can locally configure inputs and outputs for temporary use during commissioning of the device. You can configure inputs and outputs that have not been configured through WorkStation.
Więcej informacji zawiera Configure Inputs and Outputs for Temporary Use .
Display | |
Display resolution
|
128 x 64 pixels
|
Display size
|
36 W x 17 H mm (1.4 W x 0.7 H in.)
|
Display type
|
FSTN monochrome LCD, white color transflective backlight
|