earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 警报
产品版本: 2.0, 2.1, 3.0, 3.1
2018/5/18

Saving a Notification Written to a File

You save a notification written to a file in a different location, for example, to store the file or to include the file in an email message.

显示更多
action_close

The write to file notification is written to a text file when the configured notification condition is met.

You can configure whether new information is appended to the existing file, overwrites the current content of the file, or if it is written to a unique file. By default, new information is appended to the existing file. If the file does not exist, a new text file is created.

You can make the file name dynamic by replacing it with a string variable whose value you control from a program.

The text file is saved in the EcoStruxure Building Operation database folder: '...db/notifications'. You can access the notification file from the WorkStation 'System' folder, 'Notification files' subfolder of the EcoStruxure BMS server where the file was generated. You can open the notification file with a text editor installed on the computer.

You can save the file to a different location and rename it. You can also delete the notification file.

重要:

When you delete the notification file, it is deleted from the physical device.

To save a notification written to a file
  1. In WorkStation, in the System Tree pane, expand the System folder.

  2. Expand the Notification Files folder.

  3. In the List view, select the notification file you want to save to a different location.

  4. On the Actions menu, click Save as .

  5. In the Save As dialog box, select the folder where you want to save the notification file and type a name for the file.

  6. Click Save .

You can now attach the notification file to an email message or save it to an external storage device.

  • Write to File Notification Distribution Method
  • Notifications
  • Accessing a Notification Written to a File
  • Deleting a Notification Written to a File