Funkcje: Alarmy
Wersja produktu: 3.2, 3.3, 2022
2020-10-15

Deleting a Notification Written to a File

You delete a notification written to a file on an EcoStruxure BMS server to free up space.

Pokaż więcej
action_close

The write to file notification is written to a text file or to an XLSX file when the configured notification condition is met.

You can configure whether new information is appended to the existing file, overwrites the current content of the file, or if it is written to a unique file. By default, new information is appended to the existing file. If the file does not exist, a new text file is created.

You can make the file name dynamic by replacing it with a string variable whose value you control from a program.

The text file or an XLSX file, or a PDF file is saved in the EcoStruxure Building Operation database folder: '...db/notifications'. This location cannot be changed.

You access the notification file from the WorkStation 'System' folder, 'Notification files' subfolder of the EcoStruxure BMS server where the file was generated. You can open the notification file with a text editor or an XLSX file editor, or a PDF file reader installed on the computer.

You can save the notification file, from the WorkStation 'System' folder, 'Notification files' subfolder, to a different location and rename it. You can also delete the notification file.

Uwaga

When you delete the notification file, it is deleted from the physical device.

To delete a notification written to a file
  1. In WorkStation, in the System Tree pane, expand the System folder.

  2. Expand the Notification Files folder.

  3. In the List view, select the notification file(s) you want to delete.

  4. Press Delete on the keyboard.

  5. In the Confirm Delete dialog box, click Yes .

When you delete the notification file, it is deleted from the physical device.

  • Write to File Notification Distribution Method
  • Notifications
  • Accessing a Notification Written to a File
  • Saving a Notification Written to a File