earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-B, IP-IO , MP-C
功能: 硬件
产品版本: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024
2021/7/22

View Inputs and Outputs

Using the override display, you can view the configuration and the present values for inputs and outputs, and for outputs you can also view the override status.

Icons on the screens indicate the configuration and override status for the inputs and outputs. 有关更多信息,请参阅 Icons .

The value presented for an input or output equals the value transferred in or out to/from the physical device. So even if WorkStation is configured to invert a value from a counter input, digital input, digital output, or digital pulsed output, the override display presents the not inverted value.

 
action_zoom_plus_stroke I/O List screen showing configuration, values, and override status for digital outputs
图: I/O List screen showing configuration, values, and override status for digital outputs
  • SmartX AS-B Servers
  • MP-Cs
  • Output Override Function
  • Viewing Inputs and Outputs
  • Icons
  • I/O List Screen