Using the override display, you can view the configuration and the present values for inputs and outputs, and for outputs you can also view the override status.
Icons on the screens indicate the configuration and override status for the inputs and outputs.
Więcej informacji zawiera Icons
.
The value presented for an input or output equals the value transferred in or out to/from the physical device. So even if WorkStation is configured to invert a value from a counter input, digital input, digital output, or digital pulsed output, the override display presents the not inverted value.
action_zoom_plus_stroke
Rysunek:
I/O List screen showing configuration, values, and override status for digital outputs