Use the icons on the override display screens to view the configuration and the present values of the I/O points.
Icon | Description |
Input Indicates that an I/O point is configured as an input point. | |
Output Indicates that an I/O point is configured as an output point. | |
Unconfigured Indicates that an I/O point is unconfigured. | |
Input locally configured Indicates that an input point is locally configured through the override display. | |
Output locally configured Indicates that an output point is locally configured through the override display. | |
Open Indicates that a digital input point or digital output point is inactive (off). | |
Closed Indicates that a digital input point or digital output point is active (on). | |
Short-circuit Indicates a short-circuit for a universal input/output that is configured as a supervised input point. | |
Open circuit Indicates an open circuit for a universal input/output that is configured as a supervised input point. | |
Digital pulsed output Indicates that a digital output is configured as a digital pulsed output point. | |
Tristate outputs: On Indicates that a pair of digital outputs is configured as tristate output points and that the first output point is active (on) and the second output point is inactive (off). | |
Tristate outputs: Off Indicates that a pair of digital outputs is configured as tristate output points and that both the first and second output point are inactive (off). | |
Tristate outputs: -On Indicates that a pair of digital outputs is configured as tristate output points and that the first output point is inactive (off) and the second output point is active (on). | |
Tristate pulsed outputs Indicates that a pair of digital outputs is configured as tristate pulsed output points. | |
Hand Indicates that an output point is manually overridden. | |
Edit Indicates that an output point's control mode and override value can be changed. |