earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interface utilisateur

Interface utilisateur


Produits : AS-B, IP-IO , MP-C
Fonctionnalités : Matériel
Version produit : 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024, 7.0
13/03/2019

Icons

Use the icons on the override display screens to view the configuration and the present values of the I/O points.

Table : Icons

Icon

Description

 
action_zoom_plus_stroke

Input

Indicates that an I/O point is configured as an input point.

 
action_zoom_plus_stroke

Output

Indicates that an I/O point is configured as an output point.

 
action_zoom_plus_stroke

Unconfigured

Indicates that an I/O point is unconfigured.

 
action_zoom_plus_stroke

Input locally configured

Indicates that an input point is locally configured through the override display.

 
action_zoom_plus_stroke

Output locally configured

Indicates that an output point is locally configured through the override display.

 
action_zoom_plus_stroke

Open

Indicates that a digital input point or digital output point is inactive (off).

 
action_zoom_plus_stroke

Closed

Indicates that a digital input point or digital output point is active (on).

 
action_zoom_plus_stroke

Short-circuit

Indicates a short-circuit for a universal input/output that is configured as a supervised input point.

 
action_zoom_plus_stroke

Open circuit

Indicates an open circuit for a universal input/output that is configured as a supervised input point.

 
action_zoom_plus_stroke

Digital pulsed output

Indicates that a digital output is configured as a digital pulsed output point.

 
action_zoom_plus_stroke

 
action_zoom_plus_stroke

Tristate outputs: On

Indicates that a pair of digital outputs is configured as tristate output points and that the first output point is active (on) and the second output point is inactive (off).

 
action_zoom_plus_stroke

 
action_zoom_plus_stroke

Tristate outputs: Off

Indicates that a pair of digital outputs is configured as tristate output points and that both the first and second output point are inactive (off).

 
action_zoom_plus_stroke

 
action_zoom_plus_stroke

Tristate outputs: -On

Indicates that a pair of digital outputs is configured as tristate output points and that the first output point is inactive (off) and the second output point is active (on).

 
action_zoom_plus_stroke

 
action_zoom_plus_stroke

Tristate pulsed outputs

Indicates that a pair of digital outputs is configured as tristate pulsed output points.

 
action_zoom_plus_stroke

Hand

Indicates that an output point is manually overridden.

 
action_zoom_plus_stroke

Edit

Indicates that an output point's control mode and override value can be changed.

  • Output Override Function