earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-B
Funcionalidades: Hardware
Versión del producto: 1.8, 1.9
10/06/2016

I/O Filter Screen

Use the I/O Filter screen to get information on the number of inputs, outputs, and manually overridden outputs, and to filter the I/O List screen on inputs, outputs, and manually overridden outputs.

 
action_zoom_plus_stroke I/O filter screen
Figura: I/O filter screen

Tabla: I/O Filter Screen

Component

Description

IN

Select to filter the I/O List screen on inputs.

OUT

Select to filter the I/O List screen on outputs.

HAND

Select to filter the I/O List screen on manually overridden outputs.

ALL

Select to display all inputs and outputs on the I/O List screen.

Count

Displays the following numbers:

  • IN: The number of I/O points that are configured as inputs.

  • OUT: The number of I/O points that are configured as outputs.

  • HAND: The portion of the outputs that are manually overriden.

  • ALL: The total number of I/O points, including unconfigured I/O points.

  • Override Outputs
  • View Inputs and Outputs
  • Icons