earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-B, IP-IO , MP-C
Funcionalidades: Hardware
Versión del producto: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024, 7.0
13/03/2019

I/O List Screen

Use the I/O List screen to navigate through the list of I/O points, identify their configuration, view their present values, and identify if an I/O point has a manual override or not.

 
action_zoom_plus_stroke I/O list screen
Figura: I/O list screen

Tabla: I/O List Screen

Component

Description

I/O point

Displays the I/O points in a list. 

Displays a flashing highlighted I/O point when you are in configuration mode.

Configuration

Indicates if and how the I/O point is configured. Para obtener más información, consulte Icons .

Active value

Displays the present value of the I/O point.

Manual override

Indicates if an output has a manual override or not.

Scroll bar

Indicates where on the I/O list you are located.

  • Override Outputs
  • Configure Inputs and Outputs for Temporary Use
  • View Inputs and Outputs
  • Icons