earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, IP-IO , MP-C
功能: 硬件
产品版本: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024, 7.0
2019/3/13

I/O List Screen

Use the I/O List screen to navigate through the list of I/O points, identify their configuration, view their present values, and identify if an I/O point has a manual override or not.

 
action_zoom_plus_stroke I/O list screen
图: I/O list screen

表格: I/O List Screen

Component

Description

I/O point

Displays the I/O points in a list. 

Displays a flashing highlighted I/O point when you are in configuration mode.

Configuration

Indicates if and how the I/O point is configured. 有关更多信息,请参阅 Icons .

Active value

Displays the present value of the I/O point.

Manual override

Indicates if an output has a manual override or not.

Scroll bar

Indicates where on the I/O list you are located.

  • Override Outputs
  • Configure Inputs and Outputs for Temporary Use
  • View Inputs and Outputs
  • Icons