earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-B, IP-IO , MP-C
Funcionalidades: Hardware
Versión del producto: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024
19/06/2023

Output Override Screen

Use the Output Override screen to manually override an output or to remove an override for an output.

Advertencia Advertencia

Unintended equipment operation

Do not override outputs without knowing the effect.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

 
action_zoom_plus_stroke Output override screen
Figura: Output override screen

Tabla: Output Override Screen

Component

Description

I/O point

Displays the selected I/O point.

Active value

Displays the present value of the I/O point.

Configuration

Indicates that the I/O point is an output.

Edit

Indicates that the control mode and override value can be changed.

Active mode

Indicates what control mode the I/O point is in.

Mode

Displays the available control modes.

Manual override

Indicates if an output has a manual override or not.

Hand value

Select the manual override value.

Auto value

Displays the program controlled value.

  • Override Outputs
  • Icons