earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B
功能: 硬件
产品版本: 1.8, 1.9
2016/6/10

Output Override Screen

Use the Output Override screen to manually override an output or to remove an override for an output.

 
action_zoom_plus_stroke Output override screen
图: Output override screen

表格: Output Override Screen

Component

Description

I/O point

Displays the selected I/O point.

Active value

Displays the present value of the I/O point.

Configuration

Indicates that the I/O point is an output.

Edit

Indicates that the control mode and override value can be changed.

Active mode

Indicates what control mode the I/O point is in.

Mode

Displays the available control modes.

Manual override

Indicates if an output has a manual override or not.

Hand value

Select the manual override value.

Auto value

Displays the program controlled value.

  • Override Outputs
  • Icons