earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B
Functionalities: Hardware
Product version: 1.8, 1.9
11/23/2016

I/O Configuration Screen

Use the I/O Configuration screen to locally configure inputs and outputs, to go to the About screen or Status screen, and to exit the configuration mode.

 
action_zoom_plus_stroke I/O configuration screen
Figure: I/O configuration screen

Table: I/O Configuration Screen

Component

Description

IO Configuration

Select to locally configure inputs and outputs.

About

Select to go to the About screen. For more information, see About Screen .

Status

Select to go to the Status screen. For more information, see Status Screen .

Exit

Select to exit the configuration mode and return to the Home screen.

  • Configure Inputs and Outputs for Temporary Use
  • About Screen
  • Status Screen
  • Home Screen