earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, IP-IO , MP-C
功能: 硬件
产品版本: 2.0, 2.1, 3.0, 3.1, 3.2
2019/3/13

I/O Configuration Screen

Use the I/O Configuration screen to locally configure inputs and outputs, to go to the About screen or Status screen, and to exit the configuration mode.

 
action_zoom_plus_stroke I/O configuration screen
图: I/O configuration screen

表格: I/O Configuration Screen

Component

Description

IO Configuration

Select to locally configure inputs and outputs.

About

Select to go to the About screen.

有关更多信息,请参阅 About Screen on SmartX AS-B Servers .

有关更多信息,请参阅 About Screen on MP-C or IP-IO Module .

Status

Select to go to the Status screen (on SmartX AS-B servers). 有关更多信息,请参阅 Status Screen on SmartX AS-B Servers .

Exit

Select to exit the configuration mode and return to the Home screen.

  • Configure Inputs and Outputs for Temporary Use
  • About Screen on SmartX AS-B Servers
  • About Screen on MP-C or IP-IO Module
  • Status Screen on SmartX AS-B Servers
  • Home Screen on SmartX AS-B Servers
  • Home Screen on MP-C or IP-IO Module