earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-B
Funcionalidades: Hardware
Versión del producto: 1.8, 1.9
10/06/2016

I/O Selection Screen

Use the I/O Selection screen to locally configure an input or output or to remove a local configuration for an input or output.

 
action_zoom_plus_stroke I/O selection screen
Figura: I/O selection screen

Tabla: I/O Selection Screen

Component

Description

Unconfigured

Select to remove a local configuration for an input or output.

IN

Select to locally configure an input.

OUT

Select to locally configure an output.

  • Configure Inputs and Outputs for Temporary Use