earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interface de utilizador

Interface de utilizador


Produtos: AS-B, IP-IO , MP-C
Funcionalidades: Hardware
Versão do produto: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024
13-03-2019

I/O Selection Screen

Use the I/O Selection screen to locally configure an input or output or to remove a local configuration for an input or output.

 
action_zoom_plus_stroke I/O selection screen
Imagem: I/O selection screen

Tabela: I/O Selection Screen

Component

Description

Unconfigured

Select to remove a local configuration for an input or output.

IN

Select to locally configure an input.

OUT

Select to locally configure an output.

  • Configure Inputs and Outputs for Temporary Use