earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, IP-IO , MP-C
功能: 硬件
产品版本: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024, 7.0
2019/3/13

I/O Selection Screen

Use the I/O Selection screen to locally configure an input or output or to remove a local configuration for an input or output.

 
action_zoom_plus_stroke I/O selection screen
图: I/O selection screen

表格: I/O Selection Screen

Component

Description

Unconfigured

Select to remove a local configuration for an input or output.

IN

Select to locally configure an input.

OUT

Select to locally configure an output.

  • Configure Inputs and Outputs for Temporary Use