earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-B, IP-IO , MP-C
Funcionalidades: Hardware
Versión del producto: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024
13/03/2019

Digital Output Configuration Screen

Use the Digital Output Configuration screen to configure a digital output point, a digital pulsed output point, a pair of tristate output points, or a pair of tristate pulsed output points.

 
action_zoom_plus_stroke Digital output configuration screen
Figura: Digital output configuration screen

Tabla: Digital Output Configuration Screen

Component

Description

Digital

Select to configure a digital output point.

Digital Pulsed

Select to configure a digital pulsed output point.

Tristate

Select to configure the selected output point and the next output point as a pair of tristate output points.

Tristate Pulsed

Select to configure the selected output point and the next output point as a pair of tristate pulsed output points.

  • Configure Inputs and Outputs for Temporary Use