Produkty: AS-B, IP-IO , MP-C
Funkcje: Sprzęt
Wersja produktu: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024, 7.0
2019-03-13

Digital Output Configuration Screen

Use the Digital Output Configuration screen to configure a digital output point, a digital pulsed output point, a pair of tristate output points, or a pair of tristate pulsed output points.

 
action_zoom_plus_stroke Digital output configuration screen
Rysunek: Digital output configuration screen

Tabela: Digital Output Configuration Screen

Component

Description

Digital

Select to configure a digital output point.

Digital Pulsed

Select to configure a digital pulsed output point.

Tristate

Select to configure the selected output point and the next output point as a pair of tristate output points.

Tristate Pulsed

Select to configure the selected output point and the next output point as a pair of tristate pulsed output points.

  • Configure Inputs and Outputs for Temporary Use