Produkty: AS-B, IP-IO , MP-C
Funkcje: Sprzęt
Wersja produktu: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024, 7.0
2023-04-04

Pulse Period Configuration Screen

Use the Pulse Period Configuration screen to configure a pulse period for a digital pulsed output or tristate pulsed output.

 
action_zoom_plus_stroke Pulse period configuration screen
Rysunek: Pulse period configuration screen

Tabela: Pulse Period Configuration Screen

Component

Description

Period

Select a pulse period in seconds to use for the digital pulsed output or tristate pulsed output.

  • Configure Inputs and Outputs for Temporary Use