earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-B, IP-IO , MP-C
Funcionalidades: Hardware
Versión del producto: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024, 7.0
13/03/2019

Universal Input/Output Configuration Screen

Use the Universal Input/Output Configuration screen to locally configure a digital input, counter input, voltage input, temperature input, resistive input, 2-wire RTD input, supervised input, or current input.

 
action_zoom_plus_stroke Universal input/output configuration screen
Figura: Universal input/output configuration screen

Tabla: Universal Input/Output Configuration Screen

Component

Description

Digital

Select to configure a digital input.

Counter

Select to configure a counter input.

Voltage

Select to configure a voltage input.

Temp Sensor

Select to configure a temperature input.

Resistance

Select to configure a resistive input.

2-Wire RTD

Select to configure a 2-wire RTD input.

Supervised

Select to configure a supervised input.

Current

Select to configure a current input.

  • Configure Inputs and Outputs for Temporary Use