earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, IP-IO , MP-C
Functionalities: Hardware
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024
7/22/2021

Supervised Input Configuration Screen

Use the Supervised Input Configuration screen to configure a supervised circuit type to use for a supervised input.

 
action_zoom_plus_stroke Supervised input configuration screen
Figure: Supervised input configuration screen

Table: Supervised Input Configuration Screen

Component

Description

NO Series

Select to use a Normally Open (NO) circuit with a resistor connected in series with the switch.

NC Series

Select to use a Normally Closed (NC) circuit with a resistor connected in series with the switch.

NO Parallel

Select to use a Normally Open (NO) circuit with a resistor connected in parallel with the switch.

NC Parallel

Select to use a Normally Closed (NC) circuit with a resistor connected in parallel with the switch.

NO Series/Parallel

Select to use a Normally Open (NO) circuit with one resistor connected in series with the switch and one resistor connected in parallel with the switch.

NC Series/Parallel

Select to use a Normally Closed (NC) circuit with one resistor connected in series with the switch and one resistor connected in parallel with the switch.

  • Configure Inputs and Outputs for Temporary Use