earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B
功能: 硬件
产品版本: 1.8, 1.9
2016/6/10

Supervised Input Configuration Screen

Use the Supervised Input Configuration screen to configure a supervised circuit type to use for a supervised input.

 
action_zoom_plus_stroke Supervised input configuration screen
图: Supervised input configuration screen

表格: Supervised Input Configuration Screen

Component

Description

NO Series

Select to use a Normally Open (NO) circuit with a resistor connected in series with the switch.

NC Series

Select to use a Normally Closed (NC) circuit with a resistor connected in series with the switch.

NO Parallel

Select to use a Normally Open (NO) circuit with a resistor connected in parallel with the switch.

NC Parallel

Select to use a Normally Closed (NC) circuit with a resistor connected in parallel with the switch.

NO Series/Parallel

Select to use a Normally Open (NO) circuit with one resistor connected in series with the switch and one resistor connected in parallel with the switch.

NC Series/Parallel

Select to use a Normally Closed (NC) circuit with one resistor connected in series with the switch and one resistor connected in parallel with the switch.

  • Configure Inputs and Outputs for Temporary Use