Produkty: AS-B, IP-IO , MP-C
Funkcje: Sprzęt
Wersja produktu: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024, 7.0
2019-03-13

Supervised Resistor Configuration Screen

Use the Supervised Resistor Configuration screen to configure a resistor value of a supervised circuit for use with a supervised input.

 
action_zoom_plus_stroke Supervised resistor configuration screen
Rysunek: Supervised resistor configuration screen

Tabela: Supervised Resistor Configuration Screen

Component

Description

Resistor

Select a resistor value in ohm to use for the supervised input.

  • Configure Inputs and Outputs for Temporary Use