In the system example, we have created Building A and Building B with a number of identical rooms. We have also created a folder for the repeption area in Building A. In the Reception folder, we have created an analog value and a trend log that logs the temperature in the reception area. The value is connected to an alarm. A notification report that contains the log data is to be displayed in a web browser when a user manually triggers the notification.
We have created a variable triggered notification.
We have created a notification report template. The notification report template functions as a template for how notification report content is displayed when the notification is triggered. Więcej informacji zawiera Notification Reports .
The template is configured to be displayed as a simple web page that lists the temperature data in an HTML table.
The trend report data is configured to display each log record as a new table row with two cells: Timestamp and Value.
We have created a variable triggered notification.
The notification is configured to distribute the notification report as a write to file notification with the HTML file extension. The notification report is generated when a user manually triggers the variable triggered notification that uses the notification report template.
The file is accessed from the 'Notification Files' folder of the 'System' folder and is opened in a web browser.