Productos AS-B, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Alarmas
Versión del producto: 3.2, 3.3, 2022
15/10/2020

Accessing a Notification Written to a File

You access a notification written to a file on an EcoStruxure BMS server to read the contents.

Mostrar más
action_close

The write to file notification is written to a text file or to an XLSX file when the configured notification condition is met.

You can configure whether new information is appended to the existing file, overwrites the current content of the file, or if it is written to a unique file. By default, new information is appended to the existing file. If the file does not exist, a new text file is created.

You can make the file name dynamic by replacing it with a string variable whose value you control from a program.

The text file or an XLSX file, or a PDF file is saved in the EcoStruxure Building Operation database folder: '...db/notifications'. This location cannot be changed.

You access the notification file from the WorkStation 'System' folder, 'Notification files' subfolder of the EcoStruxure BMS server where the file was generated. You can open the notification file with a text editor or an XLSX file editor, or a PDF file reader installed on the computer.

You can save the notification file, from the WorkStation 'System' folder, 'Notification files' subfolder, to a different location and rename it. You can also delete the notification file.

Aviso

When you delete the notification file, it is deleted from the physical device.

To access a notification written to a file
  1. In WorkStation, in the System Tree pane, expand the System folder.

  2. Expand the Notification Files folder.

  3. Click the file.

The file is opened in a text editor.

  • Write to File Notification Distribution Method
  • Notifications
  • Saving a Notification Written to a File
  • Deleting a Notification Written to a File