earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Alarms
Product version: 2024, 7.0
3/22/2024

Create Alarm Decoration Rule Wizard - Presentation Page

Use the Presentation page or tab to configure the presentation properties when the alarm decoration rule conditions are met.

 
action_zoom_plus_stroke Presentation page
Figure: Presentation page

Table: Presentation Page or Tab

Property

Description

Override

Select the boxes for the alarm presentation properties you want to override when the alarm decoration rule conditions are met.

Alarm text message

Type the message to display when the alarm is in Alarm state and the alarm decoration rule conditions are met.

For more information, see Alarm Messages .

Category

Enter the category that the alarm belongs to when the alarm decoration conditions are met.

For more information, see Categories .

Category 2

Enter the category that the alarm belongs to when the alarm decoration conditions are met.

For more information, see Categories .

Prefix for alarm source name

Type a prefix that is added to the beginning of the source name property of an alarm record.

Priority

Enter the priority level of the alarm.

For more information, see Alarm Priority .

Auto hide

Select to automatically hide the alarm in the Alarms pane or Alarm View.

Flashing alert

Select to make the alarm row flash in the Alarms pane and Alarm Views when the alarm is triggered.

Audible alert

Select to make the alert audible when the alarm is triggered.

Custom audio

Identifies the custom audio that will sound when an alarm transition occurs.

Disable state-change logging

Select to prevent an alarm state change from creating an event.

Individual acknowledgement

Select to create a new record for each alarm transition.

Background color

Enter the background color of the row for triggered alarms in the Alarms pane and Alarm Views when the alarm decoration rule conditions are met.

For more information, see Alarm Styles View .

Font color

Enter the font color to use for triggered alarms in the Alarms pane and Alarm Views when the alarm decoration rule conditions are met.

For more information, see Alarm Styles View .

Font

Enter the font to use for triggered alarms in the Alarms pane and Alarm Views when the alarm decoration rule conditions are met.

For more information, see Alarm Styles View .

Change Control Signature

Select the change control signature to be in effect.

For more information, see Change Control .

  • Alarm Decoration
  • Alarm Messages
  • Categories
  • Alarm Priority
  • Alarm Styles View
  • Create Object Dialog – Naming the Object Page
  • Create Alarm Decoration Rule Wizard - Filter Page
  • Create Alarm Decoration Rule Wizard - User Action Page
  • Create Alarm Wizard – Attachment Page
  • Alarms Substitution Codes