earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 警报
产品版本: 2.0, 2.1, 3.0, 3.1
2018/12/17

Create Alarm Decoration Rule Wizard - Presentation Page

Use the Presentation page or tab to configure the presentation properties when the alarm decoration rule conditions are met.

 
action_zoom_plus_stroke Presentation page
图: Presentation page

表格: Presentation Page or Tab

Property

Description

Override

Select the boxes for the alarm presentation properties you want to override when the alarm decoration rule conditions are met.

Alarm text message

Type the message to display when the alarm is in Alarm state and the alarm decoration rule conditions are met.

有关更多信息,请参阅 Alarm Messages .

Category

Enter the category that the alarm belongs to when the alarm decoration conditions are met.

有关更多信息,请参阅 Categories .

Prefix for alarm source name

Type a prefix that is added to the beginning of the source name property of an alarm record.

Priority

Enter the priority level of the alarm.

有关更多信息,请参阅 Alarm Priority .

Auto hide

Select to automatically hide the alarm in the Alarms pane or Alarm View.

Flashing alert

Select to make the alarm row flash in the Alarms pane and Alarm Views when the alarm is triggered.

Audible alert

Select to make the alert audible when the alarm is triggered.

Disable state-change logging

Select to prevent an alarm state change from creating an event.

Background color

Enter the background color of the row for triggered alarms in the Alarms pane and Alarm Views when the alarm decoration rule conditions are met.

有关更多信息,请参阅 Alarm Styles View .

Font color

Enter the font color to use for triggered alarms in the Alarms pane and Alarm Views when the alarm decoration rule conditions are met.

有关更多信息,请参阅 Alarm Styles View .

Font

Enter the font to use for triggered alarms in the Alarms pane and Alarm Views when the alarm decoration rule conditions are met.

有关更多信息,请参阅 Alarm Styles View .

  • Alarm Decoration
  • Alarm Messages
  • Categories
  • Alarm Priority
  • Alarm Styles View
  • Create Object Wizard – Naming the Object Page
  • Create Alarm Decoration Rule Wizard - Filter Page
  • Create Alarm Decoration Rule Wizard - User Action Page
  • Create Alarm Wizard – Attachment Page
  • Alarm Substitution Codes