earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Alarms
Product version: 2023, 2024
12/16/2022

Create Alarm Decoration Rule Wizard - User Action Page

Use the User Action page or tab configure the user action required when the alarm decoration rule conditions are met.

 
action_zoom_plus_stroke User Action page
Figure: User Action page

Table: User Action Page or Tab

Property

Description

Override

Select the boxes for the user action properties you want to override when the alarm decoration rule conditions are met.

Cause note group

Enter the cause note group that is used by the alarm when the alarm decoration rule conditions are met.

For more information, see User Actions .

Action note group

Enter the action note group that is used by the alarm when the alarm decoration rule conditions are met.

For more information, see User Actions .

Checklist

Enter the checklist that belongs to the alarm when the alarm decoration rule conditions are met.

For more information, see User Actions .

Required User Actions

Select what actions the user has to perform when any of the listed events occur and when the alarm decoration rule conditions are met.

For more information, see User Actions .

  • Alarm Decoration
  • User Actions
  • Create Object Dialog – Naming the Object Page
  • Create Alarm Decoration Rule Wizard - Filter Page
  • Create Alarm Decoration Rule Wizard - Presentation Page
  • Create Alarm Wizard – Attachment Page