You create an alarm decoration rule to override one or several properties of an alarm when the conditions of the alarm decoration rule are met.
In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.
Click the Control Panel tab.
Under Alarm , click Decoration .
In the Alarm Decoration view, click the Add decoration button
In the Create Object wizard, in the Name box, type a name for the alarm decoration rule.
In the Path box, view the path to the location where the alarm decoration rule is stored.
In the Description box, type a description for the alarm triggered notification.
Click Next .
Click Add condition
In the Add/Remove Conditions dialog box, select the conditions.
Click OK .
In the Presentation page, select the Override boxes for the alarm presentation properties you want to override when the alarm decoration rule conditions are met.
Complete the following steps:
In the Alarm text message box, type the message to display when the alarm decoration rule conditions are met.
In the Category box, type the path to the category the alarm is to belong to when the alarm decoration rule conditions are met.
In the Category 2 box, type the path to the category the alarm is to belong to when the alarm decoration rule conditions are met.
In the Prefix for alarm source name box, type a prefix that is to be added to the alarm source name when the alarm decoration rule conditions are met.
In the Priority box, enter the priority of the alarm state when the alarm decoration rule conditions are met.
Select the Auto hide box to automatically hide the alarm in the Alarms pane or Alarm Views when the alarm decoration rule conditions are met.
Select the Flashing alert box, to make the alarm flash in the Alarms pane and Alarm Views when the alarm is triggered and when the alarm decoration rule conditions are met.
Select the Audible alert box, to make the alarm sound when it is triggered and when the alarm decoration rule conditions are met.
Ihe Custom Audio box, view the custom audio file that will sound when an alarm transition occurs.
Select the Disable state-change logging box, to prevent an alarm state change from creating an event when the alarm is triggered and when the alarm decoration rule conditions are met.
Select Individual acknowledgement to list each transition to the alarm state, regardless of how many times the alarm transitions. This ensures that you must acknowledge each individual alarm instance so that you can easily monitor certain conditions that may occur repeatedly, such as temperature changes.
In the Background color box, enter the background color of the row for triggered alarms in the Alarms pane and Alarm Views when the alarm decoration rule conditions are met.
In the Font color box, enter the font color to use for triggered alarms in the Alarms pane and Alarm Views when the alarm decoration rule conditions are met.
In the Font box, enter the font to use for triggered alarms in the Alarms pane and Alarm Views when the alarm decoration rule conditions are met.
Click Next .
In the User Action page, select the Override boxes for the user action properties you want to override when the alarm decoration rule conditions are met.
In the Cause note group box, enter the path to a cause note group that you want to connect to the alarm when the alarm decoration rule conditions are met.
In the Action note group box, enter the path to an action note group that you want to connect to the alarm when the alarm decoration rule conditions are met.
In the Checklist box, enter the path to a checklist that you want to connect to the alarm when the alarm decoration rule conditions are met.
Select W hen acknowledging an alarm : Comment to force the user to add a comment to the alarm before the alarm can be acknowledged.
Select When acknowledging an alarm : Cause note to force the user to edit the connected cause note before the alarm can be acknowledged.
Select When acknowledging an alarm : Action note to force the user to edit the connected action note before the alarm can be acknowledged
Select When acknowledging an alarm : Checklist to force the user to go through the connected checklist before the alarm can be acknowledged
Select the actions for Comment , Cause note , and Action note to specify how the user should respond to the actions when the alarm decoration rule conditions are met.
Click Next .
Click the Add attachment button
If you are logged on to a field server, an attachment used in the alarm decoration rule has to be stored on that field server.
In the Select Object dialog box, select the attachment and then click Select .
Click Create .
The properties defined in the alarm decoration rule are applied on the alarm when an alarm that meets the conditions of the alarm decoration rule changes state.